Air Cylinders
Question: What is the theoretical output of the cylinder?
Question: What is the A stroke/B stroke of the dual stroke cylinder/single rod type (-XC11)?
Question: Is it possible to operate 2 (or more) cylinders simultaneously?
Question: What is the function of the cushion valve on air cylinders?
Question: What do the horizontal lines on the cylinder stroke chart on the CAD data mean?
Question: Is the seal set for the CA1 cylinder available?
Question: What is the seal kit for the CA2 cylinder?
Question: What is the difference between the CA1 cylinder and CA2 cylinder?
Question: Are there any double clevis mountings for the CQ2D20-25DM?
Question: What is the cycle life for CBG1 series