Question: What do the horizontal lines on the cylinder stroke chart on the CAD data mean?

Answer:

The crossed-out data in the cylinder stroke table indicate that it is impossible to make such combination of the cylinder and the auto switches with the 2D-CAD data (since 2 auto switches will interferes with each other). However, in reality, such product (part number) is possibly available if the mounting position of the auto switches is changed to avoid the interference. It is possible to use the 2D-CAD data of the cylinder alone with no switches. Please see the "Minimum Auto Switch Stroke" on our catalogs for more details.

Explanation of holizontal lines on the cylinder stroke chart