Automation ● Controls ● Process
Question: It is stated that the circulating fluid used in the HRS series is tap water or 15% ethylene glycol aqueous solution. Can I use tap water or deionized water?
Question: Can I directly flow fluid whose temperature I wish to control (e.g. cutting oil, seawater, etc.) from the return port of the chiller to the discharge port?