Question: What is the shore hardness of the polyurethane tubing?
Answer:
Shore hardness for most Polyurethane tubing is A 95.
List of tubing materials and shore hardness rating
Series | Material | Shore Hardness |
---|---|---|
T/TIA | Nylon 12 | D 70 |
TS/TISA | Nylon 12 | D 56 |
TU/TIUB | Polyurethane | A 95 |
TUS | Polyurethane | A 89 |
TUH | Polyurethane | D 57 |
TCU | Polyurethane | A 95 |
TFU | Polyurethane | A 95 |
TPH | Polyolefin | D 59 |
TPS | Polyolefin | D 54 |
TAS | Nylon | D 48 |
TAU | Polyurethane | A 95 |
TRS/TIRS | Flame Resistant Nylon | D 48 |
TRB | Nylon 11 / PVC | D 53 |
Last Update: 5/1/2020
Keywords: Durometer