Question: Can we stop the rotation by using the (closed center) valve?
Answer:
It is difficult to stop the rotation by using a pressure balance, since air volume of the actuator is not enough to overcome the inertial force generated from rotation of a heavy load. Therefore, please use an external stopper instead. Please note that you need to take measures to protect against sudden movement of the piston when you start operation from the intermediate stop position.