SMC Exhibits at The Clean Show – Atlanta, July 30 – August 2
Wednesday, July 27, 2022
The Clean Show is the world’s premier trade show for the laundry, dry cleaning, and textile services industries featuring working demonstrations of equipment and products for all segments of the industry, drawing exhibitors and attendees from around the world and attracting upwards of 11,000 participants from the U.S., Canada, Mexico, Brazil, Belgium, the United Kingdom, Japan, China, Australia, and New Zealand.
SMC Corporation of America will exhibit at The Clean Show 2022 in Atlanta, Georgia World Congress Center, Booth 1801 from July 30 – August 2. SMC will feature its wireless communication technology in EtherNet/IPTM protocol supporting solenoid valve manifolds as well as the latest technologies supporting Internet of Things in the industrial and processing space.
It will also debut its latest products for the commercial cleaning and laundry industries: the JSXD 2-way, SUS solenoid valves with M12 connectors and 360° coil rotation, and the JSB angle body piston valves.
SMC products on exhibit:
- EX600 Wireless Fieldbus Communication for EtherNet/IPTM Protocol – Safe, secure wireless communication within a 10-meter radius and frequency hopping every 5 msec.
- JSXD 2-way Pilot Operated Solenoid Valves for Air, Water, and Oil – The standard stainless-steel coil cover rotates 360° with superior corrosion and water resistance. Its new coil technology maximizes magnetic efficiency reducing energy consumption. An internal stopper is utilized to reduce metal noise and longer service life. Available in: NBR, FKM, and EPDM seal materials, M12 connector, and UL and cUL.
- JSB Air Operated Angle Seat Valve – The unique shaft seal technology allows for up to 5 million cycles for use with water or air at high flow rates of Cv 28. Its body material is SUS 304 with a 360° rotational pilot port.
- Energy Saving Solenoid Valves, New SY Series – Versatile, side, top, and bottom porting locations with built-in safety features such as back pressure check valve options. Long cycle life from 70 million up to 200 million cycles. Available in IP67 protection.
- Washdown and Environment Resistant Actuators – Designed with a flat configuration, eliminating switch grooves and holes for cushion needles to prevent pooling of liquids and allow for easy wipe down of actuator surfaces.
- Refrigerated Air Dryers – Reduces the risks of water condensate in compressed air by lowering its dew point thus mitigating moisture in automation and process equipment that will cause corrosion, rust, and pipe scale.
Exhibit Dates & Hours:
- July 30 (Sat) 10:00 – 5:00
- July 31 (Sun) 9:00 – 5:00
- Aug 1 (Mon) 9:00 – 5:00
- Aug 2 (Tues) 9:00 – 3:00
Learn more at: https://www.cleanshow.com/
About SMC Corporation of America
SMC Corporation of America, headquartered in Noblesville, IN, is a subsidiary of SMC Corporation in Japan, a comprehensive manufacturer of components for the Automation, Controls, and Process industries. Its global network consists of technical centers in Japan, the United States, Europe, and China with the corporate goal of achieving the global standard for sustainable automation by reducing overall compressed air and electrical consumption by partnering directly with all stakeholders.
Recent News
SMC Corporation Exhibits at ConAgg-IFPE in Las Vegas
Monday, March 13, 2023
SMC Exhibits at SLAS 2023 – Lab Automation in San Diego
Wednesday, February 22, 2023
SMC Exhibits at MD&M West in Anaheim, CA
Monday, February 06, 2023
SMC Breaks New Ground on Sustainable Innovations in 2023
Wednesday, February 01, 2023
SMC Exhibits at Photonics West 2023 in San Francisco
Monday, January 30, 2023
All News