Actuators with Integrated Controllers

The EQ series of electric actuators feature high performance motors with integrated controllers, as well as battery-less absolute encoders.  Not all applications require the 64 positions and finely tuned speed and acceleration / deceleration curves available from JXC controllers.  Instead, EQ integrated controllers offer a simpler 2-position solenoid mode with continuous travel from origin to the opposite end of the stroke.  A closed center mode can also be set with an intermediate position.  Motor enclosures include 3 communication LEDs and M12 metal cable connectors.  Motor control optimization helps achieve up to 60% CO2 emissions.

Actuators with Integrated Controllers