ZNC-C Series - Bernoulli Gripper with Coanda Grip

  • Reduces the impact of airflow on light-weight workpieces and adjacent workpieces
  • Prevents lateral slide when suctioning the workpiece
  • There is no risk of suctioning of powder matter adhering to the workpiece into the device and pipe, as the workpiece is suctioned while air is blown.
  • Body material: Stainless steel, Aluminum
  • With Coanda grip
  • Prevents blowing away of the workpiece before suctioning and lateral sliding of the workpiece during suctioning