Industrial Chillers Glossary
A2L Refrigerant
A classification of refrigerants (like R454C) that are "mildly flammable." While they have a low Global Warming Potential, they require specific safety handling and are generally restricted from air freight.
Accumulator
A safety tank on the compressor inlet that separates liquid refrigerant from gas, ensuring only gas enters the compressor to prevent mechanical failure.
AIM Act (U.S.)
The American Innovation and Manufacturing Act, which mandates a 15-year "phase-down" of HFC refrigerants (like R410A) to 15% of their historic levels by 2036.
Air-Cooled (A Series)
A system that uses internal fans and heat sinks to release heat into the surrounding room air. Best for "plug-and-play" use where facility water is unavailable.
Auto-tuning
A function where the chiller "learns" the thermal behavior of your specific equipment and automatically adjusts its PID settings for optimal stability.
Bypass Valve
A manual or automatic valve that allows fluid to loop back to the chiller if the external machine's valves are closed, protecting the pump from damage.
Circulating Fluid
The medium carrying the heat. Common choices include Tap Water, Deionized (DI) Water, or Ethylene Glycol (antifreeze).
Compressor
The "heart" of the chiller. It pumps refrigerant through the system, raising its pressure and temperature to facilitate heat exchange.
Controller (HED-C)
The electronic unit that houses the user interface, power supply, and communication ports for the system.
Cooling Capacity
The total amount of heat a chiller can remove per hour, typically measured in kW or Tons of Refrigeration (1 Ton = ~3.5 kW).
Condenser
The component that rejects heat. In Air-cooled models, fans blow air over fins; in Water-cooled models, facility water absorbs the heat via a heat exchanger.
Deionized (DI) Water
Water with mineral ions removed. Critical for laser optics and electrical components to prevent "arcing" or scale buildup.
DeviceNet / RS-485
Standardized communication languages that allow the chiller to "talk" to the main semiconductor tool, reporting its status and alarms in real-time.
Dry Contact
A simple "on/off" electrical signal used for basic remote control or to trigger an external alarm light (tower light) if the chiller fails.
Dual Channel
A refrigeration system with two independent water circuits. In laser applications, one channel cools the Oscillator (high-precision) and the other cools the Optical Head (standard precision).
Evaporator
Where the "cooling" happens. The refrigerant evaporates here, absorbing heat from your process fluid (water/glycol), thus lowering the fluid's temperature.
F-Gas Regulation (EU)
A European Union mandate that limits the total amount of F-gases that can be sold, pushing the industry toward natural or low-GWP alternatives.
Facility Water
The external water supply (often from a cooling tower or large building chiller) required to "sink" the heat from a water-cooled unit.
GWP (Global Warming Potential)
A measure of how much a gas contributes to global warming relative to CO2.
-
Standard: R410A (~2,088 GWP)
-
Low GWP: R454C (148 GWP)
-
Natural: CO2 (1 GWP)
Heat Exchanger
A device that transfers heat between two fluids (e.g., refrigerant and water) without them ever mixing. High-efficiency models often use Brazed Plate designs.
Heat Load
The amount of thermal energy (usually measured in Watts or kW) that the semiconductor equipment generates and the chiller must remove to maintain stability.
Heaterless Heating
A patented energy-saving method that uses the hot discharge gas from the refrigerant compressor to warm the water loop, rather than using an electric immersion heater.
IEC 60601-1
The international technical standard for the safety and essential performance of medical electrical equipment. Certain SMC chillers are certified to this standard for use in hospitals and clinics.
Immersion Pump (Sealless)
A pump design where the motor and impeller are integrated without mechanical seals. This eliminates the most common point of leakage and mechanical failure in industrial chillers.
Inverter Technology
A smart control system that adjusts the speed of the compressor, pump, and fan to match the actual heat load, significantly reducing electricity consumption. It allows the compressor, fans, and pumps to vary their speed. Unlike "On/Off" chillers, inverters match the exact cooling load, saving up to 65% in energy.
-
Double Inverter: A system where both the compressor and the pump are frequency-controlled. This allows the chiller to vary its cooling output and fluid flow simultaneously, resulting in high energy savings and precise temperature control.
-
Triple Inverter: A system that uses frequency converters to control the speeds of the compressor, fan, and pump simultaneously. This allows the chiller to "sip" power based on the actual heat load rather than running at 100% capacity.
IPX4 Rating
A weather-resistance rating (found on some HRS/HRSH models) that allows the chiller to be installed outdoors safely.
Laser Optics
The lenses and mirrors that guide the laser beam; these require slightly warmer water to prevent condensation (water droplets) from forming on the glass.
Laser Oscillator
The core component of a laser system that generates the beam; it creates the most heat and requires the coldest water.
Leakage Sensor
A safety device located at the base of the HED-H that detects the presence of liquid, triggering an immediate system shutdown to prevent chemical damage or hazards.
Low GWP (Global Warming Potential)
A measure of how much a refrigerant gas contributes to global warming. Low GWP units (using gases like R454C) are more environmentally friendly and compliant with new laws.
Low GWP Chiller
A chiller designed specifically to use eco-friendly refrigerants to comply with 2026+ environmental mandates.
MPa (Megapascal)
A metric unit of pressure. The HED series typically operates up to 0.35 MPa (approx. 50 psi), which is the maximum pressure the internal PFA tubing can safely withstand.
Oscillator (Laser Source)
The component that generates the laser beam. It is highly sensitive to heat; even minor fluctuations can change the beam's wavelength or power output.
Peltier Effect
A physical phenomenon where an electric current passing through two different semiconductors creates a temperature difference, allowing one side to get cold while the other gets hot. This "solid-state" cooling requires no moving parts or refrigerants.
PFA (Perfluoroalkoxy)
A type of high-performance fluoropolymer (similar to Teflon) known for its extreme resistance to aggressive chemicals and high-purity applications, as it does not leach ions into the fluid.
PID Temperature Control System
A PID (Proportional-Integral-Derivative) temperature control system is a closed-loop feedback mechanism that maintains a desired temperature by continuously calculating and minimizing the error between a setpoint and the current process temperature. Using three mathematical terms (P, I, and D), it provides precise, stable, and automatic control, avoiding the large, repetitive fluctuations typical of simple ON/OFF systems.
R744 (CO2 Refrigerant)
A natural refrigerant with a Global Warming Potential (GWP) of 1. It is non-flammable, non-toxic, and widely used in the INR-495 and HRZC to meet strict "Green Fab" initiatives.
Rack Mounted
Equipment designed to be installed into a standard 19-inch electronic cabinet, allowing for vertical stacking to save floor space.
SEMI Standards
Global safety and ergonomic standards required for equipment used in Semiconductor fabrication plants.
-
SEMI S2: The primary safety guideline for semiconductor manufacturing equipment. It covers everything from electrical design to chemical piping to ensure the machine is safe for a cleanroom environment.
-
SEMI S8: The "Ergonomics Guideline" that dictates the physical design of the chiller, ensuring tasks like display viewing and part replacement don't cause user strain or injury.
-
SEMI F47: The ability of the chiller to continue operating without crashing during a brief drop in facility power.
Set Point
The target temperature the user programs the chiller to maintain.
Static Pressure
The resistance to fluid flow within your piping. High-pressure pumps are required if your chiller is located far from your machine or uses very thin hoses.
Temperature Stability
The "swing" or variance from your set point. Researchers usually require ±0.1°C, while general industrial use is typically ±1.0°C.
Thermo-Chiller
A device that uses a refrigeration cycle to precisely control the temperature of a circulating fluid (coolant) to remove heat from a process or machine.
VAC (Volts Alternating Current)
The power requirement for the unit (e.g., 115VAC for standard North American wall outlets or 230VAC for industrial/international power).
Waste Heat Recovery
A feature where the heat removed from the primary cooling process is recycled to warm the secondary channel (optics), reducing the need for electric heaters.
Water-Cooled (W Series)
A system that transfers heat from the chiller into a "facility water" or "house water" loop. This is preferred in cleanrooms to avoid stirring up dust or heating the room.
Wavelength Drift
A phenomenon where a laser's color/frequency shifts because of temperature changes. High-stability chillers prevent this.
Wetted Parts
Any internal component of the chiller that comes into direct physical contact with the chemical being processed. In the HED series, these are made of PFA.
Industries
High-Frequency Induction Heating
An electromagnetic process used to rapidly and precisely heat electrically conductive materials for hardening, bonding, or melting. Pneumatic actuators precisely position workpieces or induction coils to ensure uniform heat distribution during rapid thermal processing.
Laser applications and Laser Welding
The use of concentrated beams of coherent light to cut, mark, or fuse materials with extreme precision and minimal heat deformation. Pneumatic systems provide high-purity assist gases to the cutting head and power the ultra-fast, vibration-free clamping required for microscopic weld accuracy.
Packaging
Pneumatics drive the high-speed "pick-and-place" movements, bag-clamping, and box-folding mechanisms essential for rapid-fire production lines.
PET industry
A specialized sector of the plastics market focused on the production and recycling of Polyethylene Terephthalate, primarily used for beverage containers and synthetic fibers. High-pressure pneumatic systems are the primary force used to "blow-mold" heated plastic preforms into the shape of finished bottles.
Plastic industry
Compressed air is used to actuate mold platens, eject finished parts, and transport raw resin pellets through various stages of injection or extrusion.
Printing
Pneumatic cylinders maintain precise tension on paper webs and control the engagement of ink rollers to ensure consistent image quality across thousands of cycles.
Secondary Battery Manufacturing
Specialized, "copper and zinc-free" pneumatic components handle delicate electrode materials and vacuum-seal cells in controlled dry-room environments.
Semiconductors
The high-tech sector engaged in the design and fabrication of electronic components and integrated circuits that power modern computing. Ultra-clean, non-contaminating pneumatic valves and actuators manage the flow of corrosive chemicals and move wafers with sub-millimeter precision.
Welding
Pneumatic cylinders provide the heavy, repeatable clamping force needed to hold metal components in perfect alignment during robotic or manual welding arcs.